ACTION#.SOURCEPARAM
Description
ACTION#.SOURCEPARAM is used to configure an action source. Most sources do not require this parameter. For those sources, ACTION#.SOURCEPARAM is marked NotInUse.
For sources that do require this parameter, ACTION#.SOURCE must be set before ACTION#.SOURCEPARAM. When ACTION#.SOURCE is set, the units, range, and default value of ACTION#.SOURCEPARAM are updated, and the parameter is set to its default value.
Example
This example sets up a move complete action source for motion task 7 on axis 2.
>> ACTION1.SOURCE = 10 (Move complete) >> ACTION1.SOURCEID = 2 (Axis 2) >> ACTION1.SOURCEPARAM = 7 (Motion task 7)
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-01-02-000 |
|
General Information
|
Type |
Read/Write |
| Description | Action source configuration parameter |
|
Units |
Depends on ACTION#.SOURCE |
|
Range |
Depends on ACTION#.SOURCE |
|
Default Value |
Depends on ACTION#.SOURCE |
|
Data Type |
Float |
| See Also | ACTION#.SOURCE, ACTION#.SOURCEID |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.